{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the catalog numbers for the bottom and top section, and the right and left side of the trim on catalog number HCW86TS?
Issue:
Replacement part numbers for the end and side trims of HCW86TS.

Product Line:
I-Line Panelboards

Environment:
I-Line Panelboards Accessories and Repair Parts

Resolution:
The components are: End Trim: 80104-888-50 Side Trim: 80104-250-12. The top and bottom ends and left and right sides are identical.

Note: The parts are not available for purchase separately and are interplant only. If replacement trim is needed, should get the 4 piece trim part number HCW86TS.

Schneider Electric USA