{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the wire range for the compression lugs supplied in the H12LKE2 lug kit for the heavy duty safety switches?
Issue:
Product design features

Product Line:
Heavy Duty Safety Switches

Resolution:
Each compression lug will accept (1) 500 - 750 kcmil aluminum or (1) 500 kcmil copper conductor. Four lugs are supplied per connector assembly and two connector assemblies are supplied per H12LKE2 kit. One kit will supply four compression lugs for the line and load side of one switching pole or neutral of the 1200 A switch. The compression lug supplied is an Anderson (or Hubbell) VCEL07512H1.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: