{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are the horizontal ganged meter sockets available in both ring type and ringless type?
Issue:
Product Design Drawings

Product Line:
Horizontal Gang Meter Sockets

Resolution:
Yes, the horizontal gang units are available in both ring and ringless type sockets. But horizontal gang meter sockets are approved by utility company, by catalog number, so it is important to verify with the local utility company for what they require and the catalog number approved.

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
move-arrow-top