{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the repair parts for the CH361DS, series F5 (may be shown as F05)?
Issue:
Product design repair parts

Product Line:
Canadian Heavy Duty Safety Switches

Evnironment:
Repair parts

Cause:
Maintenance

Resolution:

The repair parts for the CH361DS, series F5 (F05) are as follows. No other parts are available.
-Line Base Assembly - 4056642950 (arc suppressor not included)
-Load Base Assembly - 4056002750
-Line & Load Base mounting screw - 4020516001 (3 for line & 2 for load)
-Arc Suppressor Assembly - 4056669451
-Arc Suppressor mounting screw - 4020514501 (1 required)
-Lug Assembly - CL0306F (includes 6 lugs)
-Mechanism Assembly - 4056610750 (NOTE: Handle Coupling, Cover Interlock Defeat Coupling, and Lockplate Gaskets may also need replacing)
-Handle Coupling - 4056699850
-Cover Interlock Defeat Coupling - 4056699750
-Handle Assembly - 4056699450 (also recommend replacing Lockplate Gaskets)
-Lockplate - 4056693201 (also recommend replacing Lockplate Gaskets)
-Lockplate Gasket - 4050322802 (2 required)
-Lockplate mounting screw - 2194918121 (2 required)
-Ground Lug - 4025101652 - (2 total required)
-Ground Lug Mounting Screw - 4020513503
-Fuse Pullers - FPK03 (1 required for switch)


Schneider Electric USA

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: