Search FAQs
What is the breakdown of components for the 9421LT1 and 9421LT4 , the complete kits for door mounted operating mechanisms for a MAL, MHL, MEL, and MXL breakers?
Issue:
What is the breakdown of components for the 9421LT1 and 9421LT4 , the complete kits for door mounted operating mechanisms for a MAL, MHL, MEL, and MXL breakers?
Product Lines:
Square D Circuit Breaker, MAL, MHL, MEL, MXL
Environment:
Operating mechanisms 9421
Cause:
Need the components for the thru the door mechanisms kits
Resolution:
The 9421LT1 is made up of 9421LM1, 9421LH8 and 9421LS8. The 9421LT4 is made up of 9421LM1, 9421LH8 and 9421LS10.
9421LT1
9421LT4
What is the breakdown of components for the 9421LT1 and 9421LT4 , the complete kits for door mounted operating mechanisms for a MAL, MHL, MEL, and MXL breakers?
Product Lines:
Square D Circuit Breaker, MAL, MHL, MEL, MXL
Environment:
Operating mechanisms 9421
Cause:
Need the components for the thru the door mechanisms kits
Resolution:
The 9421LT1 is made up of 9421LM1, 9421LH8 and 9421LS8. The 9421LT4 is made up of 9421LM1, 9421LH8 and 9421LS10.
9421LT1
9421LT4
Handle Kit | ||
Part # | NEMA Rating | Trip Indication |
9421LH8 | 1, 3, 3R, 12 | Yes |
9421LH48 | 4 (Painted) | No |
9421LC48 | 4X (Chrome Plated) | No |
Shaft Kit | |
Part # | Mounting Depth (in) |
9421LS8 | 7 3/16 -11 5/8 |
9421LS10 | 7 3/16 - 22 1/4 |
Operating Mechanism |
9421LM1 |
Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: