Search FAQs
What Semi-Flush flange kit is used for all the 400amp CSED that can be Semi-Flush mounted and what depth will the flange kit install in the wall?
Issue:
Product Design Features
Product Line:
Combination Service Entrance Devices
Environment:
CSED
Resolution:
The Semi-Flush flange kit for ALL the 400amp CSED that can be Semi-Flush Mounted is catalog number FK400
The Semi-Flush kit can be installed at three different levels of depth: 3.5", 4.5" and 5.5". PLEASE SEE THE INSTRUCTIONS THAT COME WITH THE KIT FOR MOUNTING
Product Design Features
Product Line:
Combination Service Entrance Devices
Environment:
CSED
Resolution:
The Semi-Flush flange kit for ALL the 400amp CSED that can be Semi-Flush Mounted is catalog number FK400
The Semi-Flush kit can be installed at three different levels of depth: 3.5", 4.5" and 5.5". PLEASE SEE THE INSTRUCTIONS THAT COME WITH THE KIT FOR MOUNTING
Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: