{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the catalog numbers for the top and bottom interior trim pieces for weatherproof enclosure MH62WP?
Issue:
Catalog numbers for the top and bottom interior trim pieces for weatherproof enclosure MH62WP.

Product Line:
PTFDS - FD Enclosure Systems

Environment:
Circuit breaker panelboards sold and supported in the USA.

Cause:
Replacement trim pieces for the MH62WP enclosure.

Resolution:
To replace the top and bottom trim for an MH62WP, (2) 80106-510-01 metal trim pieces and (2) 80106-403-01 plastic snap in pieces are required.

Schneider Electric USA