{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Video: Do the H & J frame breaker terminal nut inserts include a screw and washer?
Issue:
Do the H & J frame breaker terminal nut inserts include a screw and washer?

Product Line:
PowerPact™ H and J frame breakers

Resolution:
Yes, kits S37425, S37444, S37427, S37445  include a 1/4 - 20 x 0.75" screw with a captive Belleville washer. Kit S37426 includes a M6 x 20mm screw and separate M6 washer and S37428 includes a M8 x 20mm screw with a separate M8 washer.

The following video provides guidance for installing Terminal Nut Kits into PowerPact™ H & J-Frame Breakers:

Schneider Electric USA