{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can Square D/Schneider supply Transformers with stainless steel enclosures? What grade of stainless steel is used? Are the enclosures painted or brushed finish? What type of hardware is supplied?
Issue:
Selection of Transformers

Product Line:
LV Transformers

Environment:
Applies to Transformers by SquareD/Schneider Electric


Cause:
Stainless Steel Transformer enclosures have varying characteristics

Resolution:
SquareD/Schneider Electric offers a complete line of stainless steel transformer enclosures, in #304 or #316 stainless material, and are painted standard ANSI 49. SquareD/Schneider Electric paints the enclosure as a value added offering. The paint provides an additional level of corrosion resistance and improved heat dissipation. The hardware used is the standard corrosion resistant hardware used on all SquareD/Schneider Electric  Low Voltage Dry Type Distribution Transformers. If the customer desires stainless steel hardware, that must be provided by the installer.


 

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: