{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the repair parts for a C2M200S Series M02?
Issue:
Product Repair parts

Product Line:
Combination Service Entrance Devices

Environment:
Repair parts

Cause:
Maintenance

Resolution:

NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field repairable:
Meter Cover Assembly - 4053414150
Main Breaker Section Cover Assembly - 7329410550
Main Breaker Section Cover Hinges - (2) X2983
Main Breaker Section Cover Hinge Mounting Screws - (2) 2159414081
Dead Front Interior Trim - 7329420201
Dead Front Interior Trim Mounting Screw - 4020513001K ( This kit contains 10 screws, but only one screw is required to secure the trim)
Dead Front Interior Trim Filler Plates - (2) QOFP
Meter Base Assembly - 4053448550 (Includes meter base, (2) line side lugs, (4) meter jaws and (4) meter jaw blade guides, (2) load side lugs (feeds QO base) and load side bussing (feeds QOM2-VH))
Meter Jaw - (4) 4052706950 (OBSOLETE - REPLACED BY 7329794850)
Meter Jaw Mounting Nuts - (4) 2342702001
Meter Jaw Blade Guide - (4) 4052761901
Left Line Side Lug Assembly - 4053408750
Right Line Side Lug Assembly - 4053408850
Meter Sealing Ring - 2920910001
Closing Cap - (2) ACP
Main Breaker - QOM2-VH type, 200A maximum
Main Breaker (QOM2-VH) Mounting Nuts - (2) 2342702001
Main Breaker - QO-VH type, 50A maximum
Main Breaker (QO-VH) Mounting Base - 4050443650, Mounting Screw 2196617201
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE


Schneider Electric USA

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: