{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Is there a padlock attachment for the C60 Multi 9 breakers?
Issue:
What available padlock attachments are offered for the C60BP, C60BPR, C60SP, C60H-DC, C60N, C60H, or C60L Multi 9 breakers?

Product Line:
Circuit breakers

Resolution:
Yes. The MG26970 padlock device attaches to the front of the breaker, accepts a 0.315" (8 mm) max diameter padlock and locks the breaker in the ON or OFF position. The M9PAF is the same, but only locks in the OFF position.

Alternatively, there are side mounting devices. There is a left hand kit (MGN26380) and right hand kit (MGN26381). This allows flexibility to use other accessories on either side of the Multi-9 device. They will accommodate padlock shackle sizes of 1/4 to 3/8" (6 - 9.5 mm).

M9PAF Install Bulletin
MG26970 Installation
Side Mounting Install Bulletin

Schneider Electric USA