{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What circuit breaker size is recommended for the TV2SEMA32A ?
Issue:
Overcurrent protection for TVSS

Product Line:
Surge Protection Devices

Environment:
EMA

Cause:
Breaker size

Resolution:
The breaker size is determined by the wire size used to connect the TVSS to the panel. It is recommended to use #10 wire with a 30 amp breaker.


CTA-ID : 2038152

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
move-arrow-top