Search FAQs
What is the part number for the latch bracket that holds the Model 6 MCC unit in place? It is usually riveted to the bucket.
Issue:
Part number for the latch bracket that holds the Model 6 MCC unit in place. That it is usually riveted to the bucket.
Product Line:
MCC unit
Environment:
Model 6 MCC unit
Cause:
Maintenance and repair parts
Resolution:
The replacement ``Pawl latch assembly`` is part number 80420-879-50. However, this is only for buckets larger than 12 inches as there is not a latch assembly installed on buckets 12`` or smaller.
Refer to attached drawing for this part.
Part number for the latch bracket that holds the Model 6 MCC unit in place. That it is usually riveted to the bucket.
Product Line:
MCC unit
Environment:
Model 6 MCC unit
Cause:
Maintenance and repair parts
Resolution:
The replacement ``Pawl latch assembly`` is part number 80420-879-50. However, this is only for buckets larger than 12 inches as there is not a latch assembly installed on buckets 12`` or smaller.
Refer to attached drawing for this part.
Released for:Schneider Electric USA
Attachment(s)
Explore more
Category:
Explore more
Category: