Search FAQs
Are the base channels on a QED2 switchboard removable? Also, are they 1.5 inches high?
Issue:
Base channel Installation, Assembly, and removal.
Product Line:
Switchboards
Environment:
NEMA PB-2, UL 891, NFPA 70 Art. 408
Cause:
In some instances it may be desirable to remove the standard base channels in order to reduce the overall height of the switchboard.
Resolution:
For seismic applications, the base channels may not be removed. The base channels are an integral part of the switchboard construction during seismic testing and are therefore required for any seismic applications. For other installations the base channels, which are bolted on, are permitted to be removed if necessary or desirable. The base channels on QED2 switchboards are 1.5 inches tall.
Base channel Installation, Assembly, and removal.
Product Line:
Switchboards
Environment:
NEMA PB-2, UL 891, NFPA 70 Art. 408
Cause:
In some instances it may be desirable to remove the standard base channels in order to reduce the overall height of the switchboard.
Resolution:
For seismic applications, the base channels may not be removed. The base channels are an integral part of the switchboard construction during seismic testing and are therefore required for any seismic applications. For other installations the base channels, which are bolted on, are permitted to be removed if necessary or desirable. The base channels on QED2 switchboards are 1.5 inches tall.
Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: