{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Video: Where is all the general information (catalog and series number, date code, torque information, etc.) for a safety switch located on the switch?
Issue:
Product Design information

Product Line:
General Duty, Heavy Duty, and Double Throw Safety Switches

Resolution:
The catalog number, the series number, the date code, and torque information along with all the standard required information for a safety switch, is located on the wiring diagram label, which can be found on the back of the front cover of the switch.
Generally, the catalog and series numbers are located in the upper left area of the label, the middle of the label has all the general specifications for the switch, and the lower area of the wiring diagram label will have the date code and UL or CSA manifest.
SEE THE BELOW SAMPLE LABEL AND THE ATTACHED VIDEO

Label example

Schneider Electric USA