Issue:
Product Design featuresProduct Line:
Meter Pak Metering Equipment
Environment:
Main lug wire size
Cause:
Application
Resolution:
The MP42200, MP43200, MPR42200, MPH42200, MPR43200, MPH43200, MP64200, MPR64200 and MPH64200, contains the standard lug kit MMLK250 and accepts as standard, the following wire size and range:
(1) 1/0 - 600kcmil Al/Cu OR (2) 1/0 - 250kcmil Al/Cu wire Per Phase and Neutral.
The Alternate(or optional) Lugs for these Meter-Pak devices are:
1) The Lug kit catalog number MMLK500 and the lugs will accommodate (2) 3/0 - 500kcmil Al/Cu wires per phase and neutral
2) The Lug kit catalog number MMLK600 and the lugs will accommodate (2) #2 - 600kcmil Al/Cu wires per phase and neutral
3) For the below alternate lugs, MUST use the lug landing kit MMSK2.
NOTE: The Anderson lugs are Compression lugs and the ILSCO lugs are Mechanical lugs.
THERE ARE NO OTHER ALTERNATE LUGS AVAILABLE FOR USE ON THE ABOVE METER-PAK CATALOG NUMBERS
The MP85200, MP86200, MPR85200, MPH85200, MPR86200 and MPH86200 contains the standard lug kit MMLK500 and accepts as standard the following wires size and range:
(2) 3/0 - 500kcmil Al/Cu wires per phase and neutral.
The Alternate(or optional) Lugs for these Meter-Pak devices are:
1) The Lug kit catalog number MMLK250 will accommodate (1) 1/0 AWG to 600 kcmil, or (2) 1/0 AWG to 250 kcmil AL/CU wire(s) per phase and neutral.
2) The Lug kit catalog number MMLK600 will accommodate (2) #2 AWG to 600 kcmil AL/CU wires per phase and neutral.
3) For the below alternate lugs, MUST use the lug landing kit MMSK2.
NOTE: The Anderson lugs are Compression lugs and the ILSCO lugs are Mechanical lugs.
THERE ARE NO OTHER ALTERNATE LUGS AVAILABLE FOR USE ON THE ABOVE METER-PAK CATALOG NUMBERS