{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the aluminum and copper compression lug part numbers and wire ranges for the PowePact H frame breakers
Issue:
Are there optional aluminum compression lugs available for HD, HG, HJ, HL circuit breakers?

Product Line:
Circuit breakers

Resolution:
For (1) conductor #6 - #2 AWG Al or Cu, part number is YA060HD (3 per pack)
For (1) conductor 1/0 - 4/0 AWG Al or Cu, part number is YA150HD (3 per pack)
For (1) conductor #6 - 1/0 AWG Cu, part number is CYA060HD (3 per pack)
For (1) conductor #4 - 2/0 AWG Cu, part number is CYA150HD (3 per pack)

Schneider Electric USA

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: