{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is included with the PKOGTJ250 ground lug kit?
Cause:
Product features

Product Line:
Circuit Breaker Enclosures

Resolution:
This is a bag assembly with two lugs, two mounting screws, two sets of labels, and installation instruction card.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: