Issue:
Low Voltage Transformers (excepting Sealed Epoxy Resin Encapsulated Transformers) by SquareD/Schneider Electric are offered in both Aluminum and Copper winding materials
Product Line:
LV Transformers
Environment:
Applies to Transformers by SquareD/Schneider Electric
Cause:
Copper wound Transformers are often specified on plans and specifications
Resolution:
Square D/Schneider Electric does not offer the copper wound Ventilated Transformers as standard. Copper wound Transformers are available from the Digest or using the Product Selector and will have ``CU`` as part of the catalog number. Square D encapsulated Transformers (Sealed Epoxy Resin Encapsulated Transformers, with enclosure types A, B & C) do have copper windings as standard.
Released for:Schneider Electric USA