{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Is the connection from the main breaker to the bus in an NQ panelboard cable or bus?
Issue:
The connection to the bus from the main breaker in an NQ panelboard is cable connection?

Product Line:
Panelboards.

Environment:
Products sold in the United states.

Cause:
Product features.

Resolution:
The connection from QBL, QDL, QGL and QJL main breakers is a cable connection since the lugs on the Q frame are not removeable.
Powerpact H frame, Powerpact J frame and all L frame main breakers are bus connected. On factory assembled panels only.

Schneider Electric USA