{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are 200% neutral, non-linear, NQ panelboards available?
Issue:
200% neutral non-linear NQ panelboard

Product Line:
NO Panelboards

Environment:
Feature clarification

Cause:
Field , or Factory installation

Resolution:
Yes for the 100A interiors use field installed  NQNL1. For the 225 ampere use NQNL2 and for the 400 ampere NQNL4
The 200% rated  Copper neutral can also be requested as a factory assembled feature as well

NOTE: With the NQNL2 Copper Neutral use a NQNL2ACCY when installing sub feed, through feed lugs or a sub feed circuit breaker.
The NQNL4 is not to be used with sub feed, feed through lugs or a sub feed circuit breaker.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: