{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can a S29370, S29371, or S37422 be used on a PowerPacT H or J frame breaker in a J250S or J250F enclosure?
Issue:
Can the padlock attachments be used with J250, NEMA 1 enclosure?

Product Line:
Circuit Breaker

Resolution:
None of these accessories are suitable for use with the J250F or J250S enclosure. A padlock hasp is provided as an integral feature on the enclosure cover.

Schneider Electric USA

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: