{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
8536SGG1 Series B starter, Series C enclosure: What is the number for the reset mechanism?
Issue:
Replacement reset mechanism for 8536SGG1

Product Line:
NEMA Contactors and Starters

Environment:
8536 Type S Starters

Resolution:
It is the 30019-113-69 (melting alloy + solid state overload), or 30019-113-64 (bimetallic overload). If the customer also needs the ring nut order 30019-121-01

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: