{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Video: What are some of the differences between the QO and HOM load centers?
Issue:
Product Features

Product Line:
QO and Homeline Load Centers

Resolution:
Below are some of the differences between the QO and Homeline load centers and branch circuit breakers;
(PoN = Plug-On Neutral)
 
Item         QO Load Centers                                            Homeline Load Centers
1)Tin plated copper bus bars            Tin plated aluminum bus bars
2)Shielded bus barsNo shielded bus bars
3)Available in single and three phaseAvailable ONLY in single phase
4)Surface and flush covers available separately Combination surface/flush cover ONLY and comes standard with load centers
5)Available in both traditional and PoN       ALL new convertible, double row construction, Homeline load centers are PoN design
6)QO PoN panels do not accept the QOT type tandems. If a QO PoN accepts tandems it will be the Old Style QO type Tandem and ONLY in certain spaces. See the Load Center Labeling                      ALL PoN panels accept tandems in all spaces
7)Split branch neutrals located at top of the interiorSplit branch neutrals distributed down both right and left sides of interiors

NOTES:
1) For differences between the QO and Homeline branch breakers, see FA321509
2) QO and Homeline are NOT interchangeable, so the QO branch breakers CANNOT be used in Homeline and the Homeline branch breakers CANNOT be used in QO

 




 

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.