undefined [object Object]
{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the required distance between hangers or how many hangers are required for I-Line II busway?
Issue:
How many feet apart do you mount hangers for the I-Line II busway?

Product Line:
Busway.

Environment:
I-line II.

Cause:
installation and mounting.

Resolution:
Indoor horizontal busway requires one hanger at least every 10 feet.
Vertical Indoor busway requires one hanger at least every 16 feet.
Outdoor Feeder Busway requires one hanger at least every 5 feet in both the vertical or horizontal orientations.

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: