{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What legend plates are used with the XACA pendant stations?
Issue:
Where to locate the legend plates used on XAC pistol grip stations?

Product Line:
Push Buttons and Operator Interface

Environment:
XAC Standard Duty Pistol Grip Stations

Resolution:
The old style ZB2BY**** 30mm X 40mm plastic legends are used with the XACA pendant stations. See Digest 178 19-135 for available legends.

Schneider Electric USA