{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
How to determine the correct weather shield, wall mounting bracket, ceiling mounting bracket, and replacement parts for a transformer?
Issue:
Enclosures and Accessories and replacement parts for a LV Transformer

Product Line:
LV Transformer

Environment:
EE and EX LV Transformer

Resolution:
Find the catalog number (or a standard catalog number that is the same kVA, temperature rise and kfactor) in the current Digest. There is a letter/number combination next to the catalog number in the Enclosure column.
Take that number (for example 20D) and turn to the page in Catalog 7400CT0601 that corresponds to the enclosure. There are dimensions and an accessories/replacement parts matrix on the page.
Note that neither voltages, shielding, frequency, winding material nor sound level impact the enclosure size. So an EE75T211HISCU47DB will be in the same enclosure as a EE75T3H. Temperature rise and kFactor DO impact enclosure size, so choose the correct standard reference unit in the Digest

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.