{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the part number for a legend plate with special engraving for the XAC pendant stations?
Issue:
How many characters can we put on the customized legend plate for the XAC pendant station?

Product Line:
Push Buttons and Operator Interface

Environment:
XACA Pendant Stations

Resolution:
Use the following part numbers and specify text:
ZB2BY2002 is a 30 x 40 mm legend black with white letters
ZB2BY2004 is a 30 x 40 mm legend red with white letters
ZB2BY4001 is a 30 x 40 mm legend white with black letters
ZB2BY4005 is a 30 x 40 mm legend yellow with black letters.

Text is limited to 2 lines of 11 characters each.

Schneider Electric USA