{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the repair parts for the H361, series F5? (may be shown as F05)
Issue:
Current Design repair parts

Product Line:
Heavy Duty Safety Switches

Resolution:
The repair parts for the H361, series F5 (F05) are as follows. No other parts are available.

Line Base Assembly - 4056642050 (1 required; arc suppressor assembly not included)
Load Base Assembly - 4056002550K (1 required)
Line and Load base mounting screws - 4020516001 (3 required for line base and 2 required for load base)
Arc Suppressor Assembly - 4056669451 (1 required)
Arc suppressor mounting screw - 4020514501 (1 required)
Lug Assembly - 4025101652 (per lug)
Lug mounting nut - 4020515401
Switch Mechanism - 4056610750
Handle Assembly - 4056684150K
Lockplate - 4056637601
Lockplate mounting screws - 2299940562 (2 required)
Cover latch and spring - 4056607201 (latch) and 4022304301 (spring)

Schneider Electric USA

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: