Search FAQs
Will a K frame breaker such as a KA, KH, KC or KI fit into an HCN panel?
Issue:
Can you install a KA, KH, KC or KI breaker into an HCN I-line panel?
Product Line:
Distribution Panelboards
Environment:
I-Line HCN panelboard
Cause:
Fit
Resolution:
No, a K frame breaker will not fit into an HCN panel. If the panel is wired to 480V, the largest branch available is a 150A H frame. If wired to 240V the largest is a Q frame breaker up to 225A.
Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: