{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are the 8910 Type DPA definite purpose contactors both UL listed and UL recognized, if so what is the UL File number?
Issue:
UL file number for the 8910 DPA devices?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Definite Purpose Contactors and Starters

Resolution:
8910 devices are UL Component Recognized as standard under UL File # E78351 CCN NLDX2. If UL Listing is desired, then add Form U1 which changes the UL File to E78351 CCN NLDX.

NOTE: If device has quick connectors, this form will cause the removal of them (at present). Form U1 does not apply to the 8910DP devices.

Schneider Electric USA