{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can the 2510 Type K be used on non motor loads such as resistance heaters?
Issue:
2510 Type K application

Product Line:
Manual Starters and Switches

Environment:
Manual Switches, 30 A—Type K

Resolution:
Yes, 30A maximum, 600VAC maximum

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.