{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can the 9999S__ cover mounted control units be used with the Class 8941 Duplex controllers?
Issue:
Can 9999S  cover mounted control units be used with Class 8941 Controllers?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Class 8941 Duplex controllers

Resolution:
Yes, select as if the controller was Class 8538 Type S .

Schneider Electric USA