Search FAQs
What screws are used to attach plastic mimic bus to switchgear?
Issue:
What is the screw part number for attaching the plastic mimic bus to HVL type gear?
Product Line:
Switchgear
Environment:
HVL, HVLcc, HVLcb
Resolution:
Corporate Part number 21594-12120. #6-32 x 3/8`` steel tap screw, Pan Head, Phillips Head, zinc yellow chromate full finish. Stainless steel screws are also used.
What is the screw part number for attaching the plastic mimic bus to HVL type gear?
Product Line:
Switchgear
Environment:
HVL, HVLcc, HVLcb
Resolution:
Corporate Part number 21594-12120. #6-32 x 3/8`` steel tap screw, Pan Head, Phillips Head, zinc yellow chromate full finish. Stainless steel screws are also used.
Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: