{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the catalog number for the handle on a LK3AR4?
Issue:
Is there a hanle available for LK3AR4 disconnect?

Product Line:
Operating Mechanisms and Disconnect Switches

Environment:
Tesys LK disconnect switches

Resolution:
No, LA8SATD6 Be aware that these switches are not promoted in the US. As a result, they meet IEC standards but not UL. (It has now been obsoleted)

Schneider Electric USA