{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Is there a shunt trip mechanism for a general duty, heavy duty, or double throw safety switch?
Issue:
Does Square D have a shunt trip device for safety switches?

Product Line:
Safety Switch

Resolution:
Safety switches are strictly a mechanically operated device. An electrically operated shunt trip mechanism is not available for the safety switch product line. For a shunt trip application, consider using an enclosed circuit breaker with a shunt trip accessory installed.

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: