{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can you use the SDSA1175 for residential or commercial use?
Issue:
Can SDSA1175 be used in a commercial application?

Product Line:
Surge Protection

Environment:
Load Center SPD

Resolution:
The SDSA1175 can be used in both Residential and Commercial applications. However, a Commercial application may require a higher AIC rating or peak surge rating than the SDSA1175 provides. Also, most commercial applications have motor, computer, or electronic loads where a TVSS unit like the HEPD, XR or HWA would be better suited and provide more protection.

Schneider Electric USA