Issue:
What does AIC stand for?
Product Line:
Circuit Breakers
Resolution:
AIC stands for "Ampere Interrupting Capacity". This term is obsolete as the industry now refers to it as AIR or "Ampere Interruption Rating". These refer to the interrupt rating of a breaker, which is the level of fault the breaker can interrupt without damage.
What does AIC stand for?
Product Line:
Circuit Breakers
Resolution:
AIC stands for "Ampere Interrupting Capacity". This term is obsolete as the industry now refers to it as AIR or "Ampere Interruption Rating". These refer to the interrupt rating of a breaker, which is the level of fault the breaker can interrupt without damage.
Released for:Schneider Electric USA