{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is a LOGK1 or LOGK2 accessory for the Heavy Duty Safety Switches?
Issue
Product design features

Product Line:
Heavy Duty Safety Swithces

Environment:
Accessories

Cause:
Application

Resolution:
LOGK1 and LOGK2 are an optional, supplemental Lock-Off Guard Kit. Installation of the lock-off guard will restrict the inadvertent insertion of a padlock into the lock plates, lock-off opening, when the handle of the switch is in the ON position.

The LOGK1 can ONLY be used on 30A/240V, 30A/600V or 60A/240V, Series F, Heavy Duty Safety Switches, NEMA 1, 3R or 12.

The LOGK2 can ONLY be used on 60A/600V, 100A/240V, 100A/600V, 200A/240V or 200A/600V,Series F05 (or newer), Heavy Duty Safety Switches, NEMA 1, 3R or 12. This kit is not compatible with Series F01 to F04 Heavy Duty switches. For Series F01 - F04 switches, the LOGK2 can be used if the existing handle/mechanism assembly is replaced with the replacement handle/mechanism kit HM0610F, Series F05 (60A and 100A switches only).

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
move-arrow-top