{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are padlocking provisions provided on the Class 2510 Type M & T manual starters?
Issue:
Are padlocking provisions already included on the Class 2510 Type M & T manual starters?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Class 2510 Type M & T manual starters

Resolution:
Yes, padlock provisions are standard on all enclosed and open style 2510 Type M & T devices. These can be padlocked in the OFF position only. NOTE: These devices do not meet the requirements for Lock Out Tag Out per the NEC, they are not UL 98 listed.

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.