{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the part number for a 200% Neutral for an NF panelboard?
Issue:
What is the part number for a 200% Neutral for an NF panelboard?

Product Line:
Panelboards.

Environment:
Products sold in the United states.

Cause:
Maintenance.

Resolution:
The part number for a 200% neutral for NF panelboards are :
100A and 125A interiors use NFNL1, 250A interiors use NFNL2, and 400A interiors use NFNL4.


CTA-ID : 2048748

Schneider Electric USA