{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are the Generator Panels QO1DM10020TRBR, QO1DM10030TRBR and QO1DM10050TRBR suitable for outdoor use?
Issue:
Application

Product Line:
QO Load Center

Cause:
Clarifying application for use outdoors.

Resolution:
Yes, these Generator Panels are rated NEMA Type 3R for use outdoors in a weatherproof application.
We do not offer an indoor, NEMA Type 1 equivalent, but the Type 3R panels can also be used indoors in a NEMA Type 1 environment.


CTA-ID : 2048796

Schneider Electric USA