undefined undefined
{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the replacement for the XBLZ pushbuttons?
Issue:
XBLZ pushbuttons replacement

Product Line:
Push Buttons and Operator Interface

Environment:
XBLZ Obsolete Push buttons

Resolution:
The XBLZ line is obsolete. They were operators and accessories used in custom keypad assemblies. There are no parts available and no direct cross. They have to replace with something in the Magellis product line which is a different form, fit and function. Contact the Automation support group at 1-800-468-5342 for assistance selecting Magellis products.

Schneider Electric USA