{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Is the 32510 a double barrel lug?
Issue:
32510 Kit is a double barrel lug

Product Line:
Panelboards and accesories

Environment:
Products sold and used in the United States

Cause:
Product Features

Resolution:
Yes. Kit includes (3) 2-barrel lugs. Each lug is suitable for (2) 2/0 AWG-350 kcmil CU, OR (2) 2/0 AWG-500 kcmil AL.


CTA-ID : 2047910

Schneider Electric USA

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: