{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the rating for Square D Wireway such as the LJB type?
Issue:
Rating available for Square D Wireway such as the LJB type

Product Line:
Square-Duct Wireways

Environment:
Products sold and used in the United States

Cause:
Product Features

Resolution:
Wireway is available in NEMA 1, 12, and 3R. The LJB wireway has a NEMA 12 rating.

Schneider Electric USA