{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the Difference Between the 9007CR53B2 and 9007CR53B?
Issue:
Needs to know if the 9007CR53B2 can be used as a replacement for the 9007CR53B.

Product Line:
Limit Switches

Environment:
9007 NEMA Limit Switches

Resolution:
The hardware is identical. The difference is in the setting of the head. Remove the head from the body and look underneath the head for the setting. On the 9007CR53B2 the setting allows the shaft to operate the contacts in either the CW and CCW direction. On the 9007CR53B the shaft only operates the contacts in the CW direction.

Schneider Electric USA