{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
How does the 8903LX latch ?
Issue:
8903LX latching operation

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Multipole Lighting Contactors, Type L and LX

Resolution:
This lighting contactor uses a mechanical latching assembly to hold the contacts in the `energized` state once power is removed from the latching coil. There is a second coil called the unlatch coil that will allow the contactor to return to the de-energized state.

Schneider Electric USA