{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are Schneider Electric QED type switchboards available with bussing that is copper with no Silver, or Tin plating?

Issue:
QED type switchboards with bussing that is copper with no Silver / Tin plating availability

Product Line:
QED SWBD

Environment:
Application

Cause:
Specification requirement

Resolution:
Bussing is not available without plating. Copper oxidizes and the oxides do not stay on the copper well. When they come off there is more copper exposed, which in  turn oxidizes, and so-on. Also the oxides do not conduct well. This causes poor electrical contact, which then gets hot and increases the oxidation rate. The oxides, because of their poor conductivity, also cause arcing at the electrical contacts, eroding the copper. oxidizes and the oxides do not stay on the copper well.

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: