{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the repair parts for an SO2040M200S, series M01?
Issue:
Current design repair parts

Product Line:
Combination Service Entrance Devices

Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field repairable:
Meter Cover Assembly - 4056185050
Meter Cover Mounting Screw - 4020513001K (contains 10 screws; only 2 required)
Meter Sealing Ring - 2920910001
Load Center Cover Assembly - 4056157550 (includes hinges and cover latch)
Load Center Cover Mounting Screws - (4) 2159417121
Dead Front Interior Trim - 4056173901
Dead Front Interior Trim Mounting Screw - 4020513001K (contains 10 screws; only 2 required)
Load Center Interior - 4056162050 (main breaker not included)
Load Center Interior Mounting Screws - (4) 2153217161
Main Breaker - QOM2200VH
Meter Base Assembly - 4056190150 (includes meter base, line side lugs, line and load side meter jaws, meter jaw blade guides, and load side connector busbars)
Meter Base Assembly Mounting Screw - 2153217161
Meter Jaw - (4) 7329794850
Meter Jaw Blade Guide - (4) 4052761901
Left Side Utility Section Barrier - 4056226601
Mounting Hardware - (2) 2159417121 screws and (1) 2430315290 rivet
Right Side Utility Section Barrier - 4056155801
Mounting Harware - (2) 2159417121 screws
Top Endwall Closing Plates - (2) ACP
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: