{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the torque specification for the phase lugs that are used on a 200 amp fusible bus plug such as a PQ4220G?
Issue:
Torque specification for the phase lugs used on PQ4220G 200 amp fusible bus plug

Product Line:
Fusible Busway

Environment:
Products sold and used in the United States

Cause:
Product Features

Resolution:
The phase lug torque values are:
Mounting hardware, torque = 80 in-lbs
Wire binding screw, torque = 275 in-lbs

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: